You are here: Using the PDMM or PCMM Controller > Using the Web Server > Using the KAS Web Server

Using the KAS Web Server

Kollmorgen Automation Suite™ comes with a web server that allows you to perform the following operations:

‡ PDMM and PCMM only

The web server may be accessed two ways:

  1. Open a web browser and enter the controller's IP address.
  2. From the Controller node in the Project tree in the KAS IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger.

The web server consists of the home page, and the KAS Application, Settings, Backup & Restore, Diagnostics and Help tabs. The Help tab is a link which opens the Web Server manual.

Figure 7-1: The Webserver Tabs as seen on an PDMM webserver.

 

Web Server Home Page

Web Server KAS Application

Web Server Settings

Backup and Restore from the Web Server

Web Server Diagnostic


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™